Media Resources
Emerson is helping our customers meet their operating, sustainability, and business performance goals. Find out how.
To meet increasing demand for greenhouse gas reduction and vital sustainability targets, companies are looking to adopt hydrogen as a flexible, renewable energy source. Emerson delivers environmentally sustainable solutions for customers across the hydrogen value chain, from production to transmission and storage, to distribution and consumption. The right technologies can help improve productivity, reduce variability, decrease energy usage, lower emissions and validate the sustainability of operations across the value chain.
Emerson is working with BayoTech, an innovator in hydrogen solutions that is producing cleaner, lower-cost hydrogen by building hundreds of modular, efficient hydrogen units. These units can produce up to 1,000 kilograms of hydrogen per day, enough to fill as many as 200 hydrogen fuel cell vehicles. To drive scale globally, BayoTech’s local production hubs will rely on Emerson’s programmable logic controller and edge control technologies, remote monitoring, and Microsoft® Azure IoT Suite to operate safely and autonomously.
“Hydrogen is regarded as the ‘fuel of the future,’ but with ambitious decarbonization targets it is essential to expand production capacity and accelerate the transition to hydrogen produced using sustainable energy.”
Mark Bulanda,
executive president of Emerson's Automation Solutions business
Frequently Asked Questions about Hydrogen
Today, 99% of all hydrogen is produced from fossil fuels such as natural gas or coal via gasification or steam methane reforming with CO2 as a byproduct. Carbon capture, utilization and storage (CCUS) technology can then be applied to remove greenhouse gases, resulting in so-called blue hydrogen. Hydrogen can also be made from electrolysis, which applies an electrical current to water molecules, splitting them into oxygen and hydrogen with zero carbon emissions. Most electrolysis is powered by the existing electricity grid, but if renewable sources such as wind or solar are used, the resulting “green” hydrogen can provide the same.
Hydrogen is an extremely versatile fuel that offers a path to sustainable long-term economic growth. It can add value to multiple sectors in the global economy by serving as a sustainable fuel for transportation and manufacturing, and an input for the production of electricity and heat for homes. Industry experts project that a $2.5 trillion global market for hydrogen technologies could exist by 2050, with 3.4 million jobs added in the U.S. alone. Furthermore, renewable hydrogen could cut global CO2 emissions by 25% if produced at scale.
But to achieve full commercialization, key challenges related to cost, durability, reliability, performance, and lack of infrastructure must be addressed. New technologies, such as electrolyzers with greater output capacity, must be further developed and expanded into larger markets for hydrogen to compete with fossil fuels or wind, solar and nuclear energy in terms of life-cycle cost, performance, durability, learning rates and environmental impact. Non-technical barriers also need to be addressed, such as developing codes and standards, establishing best practices for safety, and developing a robust supply chain and workforce.