Emerson’s wireless condition monitoring and prediction system reduces plant downtime and maintenance costs for SABIC Teesside

Emerson_502904b_SABIC_Teesside

SABIC Olefins plant in Teesside, UK

High resolution photo








MEDIA CONTACTS:
Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
[email protected]

Online vibration monitoring of pumps identifies potential problems earlier, enabling planned maintenance and greater plant availability

AUSTIN, TEXAS (April 30, 2014) -- Emerson Process Management’s wireless condition monitoring and prediction system is being used at the SABIC Olefins plant in Teesside, UK, to detect potential problems with pumps before they disrupt normal operations. The system helps reduce the risk of unexpected failures that can cause lost production and expensive repairs, as well as safety and environmental incidents.

The critical pumps being monitored are installed on the plant’s Olefins Cracker, which is used to produce ethylene, propylene, butadiene and gasoline products. SABIC Teesside previously collected and analyzed vibration data for these pumps manually, but potential problems could occur between readings. This led to higher maintenance costs and reduced plant availability, which was affecting overall production.

“We wanted to improve the monitoring of critical pumps at the Olefins plant in Teesside,” said David Hambling, Instrument Electrical Technical Engineer, SABIC UK Petrochemicals. “By installing Emerson’s wireless vibration transmitters we can now continuously monitor vibration levels and detect faults before a failure occurs.”

Emerson’s online vibration monitoring system has detected a number of problems that could have resulted in equipment failure, including a chipped tooth on a gearbox gear and an impending bearing failure. Identifying and rectifying potential problems earlier helps minimize pump failures and maintenance costs.

In addition to measuring overall vibration and temperature, the CSI 9420 Wireless Vibration Transmitter includes PeakVue™ technology, which detects faults that cause impacting, friction, and fatigue, particularly in gearbox and rolling element bearings. The monitoring system takes basic readings every 60 seconds and an in-depth, full spectrum analysis once every day. By tracking rising vibration levels, SABIC Teesside can detect developing faults and improve maintenance scheduling.

“Emerson’s Smart Wireless technologies, combined with advances in sensor technology and low lifecycle costs, have made it quick and easy for our customers to access data from their critical assets,” said Nathan Pettus, vice president, Machinery Health Management for Emerson Process Management. “With our proven predictive technologies like PeakVue and our focus on pervasive sensing, we are helping customers like SABIC Teesside to filter, automatically analyze, and capture useful, actionable information so they can rectify any issues that could interrupt production.” 

The plant’s existing Emerson Smart Wireless network made installing the wireless vibration transmitters quick and easy, enabling vibration data to be sent to SABIC’s process control system. The established mesh network also makes it easy to add or relocate wireless-enabled devices for additional process information from remote or difficult-to-access locations.

“Wireless monitoring has shown itself to be a valuable tool in our condition monitoring armory,” added SABIC’s Hambling. “Predicting failures in gearboxes of this type can make considerable savings on any subsequent turnaround and help to keep equipment available.”

Mídia:
• Contatos: Contatos de mídia global da Emerson

Outros recursos:
• Participe da comunidade Emerson Exchange 365
• Siga a Emerson no X Facebook LinkedIn YouTube

Sobre a Emerson 
Emerson (NYSE: EMR) é uma empresa global de tecnologia e software que fornece soluções inovadoras para os clientes dos mercados industrial, comercial e de consumo. Por meio de seu portfólio de automação, que é líder de mercado, além de sua participação majoritária na AspenTech, a Emerson ajuda fabricantes híbridos, de processo e discretos na otimização de suas operações, na proteção de seus funcionários, na redução de emissões e na realização de metas de sustentabilidade. Para mais informações, acesse Emerson.com.

Ative o JavaScript para usar este site.