Emerson’s wireless vibration transmitter now provides key insights into the condition of machinery located in hazardous areas

CSI9420

The CSI 9420 Wireless Vibration Transmitter is now approved for Class I, Div 1 and ATEX Zone 0 areas

High resolution photo








MEDIA CONTACT:
Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
[email protected]

CSI 9420 Wireless Vibration Transmitter is now approved for Class I, Div 1 and ATEX Zone 0 areas

AUSTIN, TEXAS (August 28, 2012) -- Emerson Process Management has expanded the application of its CSI 9420 Wireless Vibration Transmitter with intrinsic safety ratings to the US, Canadian, and European standards. With the Class I, Div 1 and ATEX Zone 0 ratings, the CSI 9420 can now be installed directly in hazardous areas such as chemical, petrochemical, and off-shore facilities as well as other explosion-classified environments.

The CSI 9420 connects quickly, easily, and economically to any machine. The safety ratings, which are in addition to existing hazardous area ratings to the Brazilian and IECEx standards, further extend the benefit of wireless technology to new areas of the plant. The CSI 9420 provides key insights into the condition of pumps, fans and other assets located in hazardous areas without the expense of running cables. 

"Our focus is to help our users make better, more informed decisions about their key production assets,” said Ron Martin, vice president/general manager of Emerson’s Asset Optimization and Lifecycle Care business. “The strength of our wireless technologies married with our machinery health expertise gives users the ability to get information that leads to timely, accurate decisions—decisions that can have profound impact on the availability and performance of their facility."

Mídia:
• Contatos: Contatos de mídia global da Emerson

Outros recursos:
• Participe da comunidade Emerson Exchange 365
• Siga a Emerson no X Facebook LinkedIn YouTube

Sobre a Emerson 
Emerson (NYSE: EMR) é uma empresa global de tecnologia e software que fornece soluções inovadoras para os clientes dos mercados industrial, comercial e de consumo. Por meio de seu portfólio de automação, que é líder de mercado, além de sua participação majoritária na AspenTech, a Emerson ajuda fabricantes híbridos, de processo e discretos na otimização de suas operações, na proteção de seus funcionários, na redução de emissões e na realização de metas de sustentabilidade. Para mais informações, acesse Emerson.com.

Ative o JavaScript para usar este site.