Emerson’s Coriolis flowmeter is MID certified for truck deliveries of cryogenic liquids

502610_a

Emerson’s Micro Motion Coriolis flowmeter is MID certified for truck deliveries of cryogenic liquids

High resolution photo


502610_b

Emerson’s Micro Motion F100 Coriolis Flowmeter provides a compact, reliable and accurate solution for cryogenic liquid re-sellers and distributors

High resolution photo








MEDIA CONTACT:
Grace Capwell
Emerson Automation Solutions
+1 (512) 834-7214
[email protected]

Micro Motion® custody transfer solution includes the Coriolis transmitter and MID-approved printer with the option of a flow computer

BOULDER, COLO (May 16, 2012) -- Emerson Process Management announces additional MID certification for its Micro Motion® Coriolis flowmeters for custody transfer. The certification covers the F100 model from the F-Series product range, for truck deliveries of cryogenic liquids, such as argon, nitrogen and oxygen. This new certificate from NMi (Nederlands Meet Instituut) adds to an already wide range of MID approvals for the measurement of liquids and gases under normal and cryogenic flow conditions.

Micro Motion Coriolis flowmeters already have European, Asian, Australian and U.S. approvals for cryogenic liquids in custody transfer applications. The flowmeters provide accurate and repeatable readings of mass flow, density, and temperature, making them ideal for critical measuring applications.

The additional certification means that Emerson can now offer cryogenic liquid re-sellers and distributors a compact, reliable and accurate solution for their delivery trucks that meets the MID requirements for direct mass flow measurement in custody transfer deliveries. The complete Micro Motion solution includes the Coriolis transmitter and MID-approved printer, with the option of a flow computer.

In detail, the certification covers the Micro Motion F100 Coriolis Flowmeter and ATEX and IECEx IIC approval, for use with cryogenic liquids with flow rates between 3.5 - 450 kg/min, densities between 700 and 1500 Kg/m3, and temperatures down to -200°C. The ambient temperature range is from -40 to +55°C. These Micro Motion Coriolis flowmeters meet the requirements of the MID guidelines; environmental class M3/E3 and accuracy class 2.5, which specify an accuracy of 1.5% for the meter and 2.5% for the complete measuring system.

All European Union countries, plus Norway and Switzerland, have committed themselves to standardize all custody transfer applications using one set of rules and guidelines. This will allow easier and smoother transfer of liquids and gases between EU member countries. By October 30,  2016, all countries are required to have the applications to comply with these rules as stated in the Measuring Instruments Directive (MID) 2004/22/EC. Cryogenic liquids also fall under these regulations.

“Emerson Process Management offers a wide range of MID approved products and MID consultancy services,” said Stephane Tritz, Vice President Flow Europe. “By providing MID certificates with products for single usage or to be integrated into a system, customers can focus their attention on their system design.”

Mídia:
• Contatos: Contatos de mídia global da Emerson

Outros recursos:
• Participe da comunidade Emerson Exchange 365
• Siga a Emerson no X Facebook LinkedIn YouTube

Sobre a Emerson 
Emerson (NYSE: EMR) é uma empresa global de tecnologia e software que fornece soluções inovadoras para os clientes dos mercados industrial, comercial e de consumo. Por meio de seu portfólio de automação, que é líder de mercado, além de sua participação majoritária na AspenTech, a Emerson ajuda fabricantes híbridos, de processo e discretos na otimização de suas operações, na proteção de seus funcionários, na redução de emissões e na realização de metas de sustentabilidade. Para mais informações, acesse Emerson.com.

Ative o JavaScript para usar este site.