Downhole Reservoir Network First to Connect Wireless Sandface Data to Upper Completion for Optimized Production

​The Roxar Downhole Matrix Wireless Interface enables a solution for wireless monitoring of the lower completion

The Roxar Downhole Matrix Wireless Interface™ enables a solution for wireless monitoring of the lower completion. High resolution image


Emerson and Metrol solve complex challenges with the wireless Intelligent Multistage Completion Network™ for reservoir insights from the sandface

STAVANGER, Norway (April 24, 2019) - Emerson, in partnership with Metrol, a leader in battery-powered wireless well monitoring, has launched the Intelligent Multistage Completion Network™ – an integrated upper and lower completions downhole solution that communicates wirelessly with instruments at the reservoir sandface, the physical interface between the formation and the wellbore. This is enabled by a new wireless interface that generates crucial zonal flow information and sandface monitoring in the lower completion.

The new solution builds on Emerson’s years of experience in advanced permanent downhole monitoring and its close collaboration with Metrol.

“For many operators, the sandface and lower completion have simply been considered ‘off limits’ for acquiring accurate multi-zone information’ – too much risk, too costly and too complex,” said Geir Aanensen, vice president and general manager for Emerson’s flow solutions business.

 “With our new wireless interface that enables connection to sandface data and flow control instruments from Metrol, operators will have unrivalled insights into the reservoir’s flow characteristics, access to valuable data and the ability to optimize reservoir production management. Combining Roxar and Metrol technologies will ensure highly efficient well and reservoir management, while providing a life-of-well, permanent hybrid silicon on insulator (HS) gauge installation.”

The Intelligent Multistage Completion Network builds on the capabilities of the existing Integrated Downhole Network that has been installed in wells worldwide and uses wireless telemetry to enable communication with sensors and controls located at the reservoir. Key benefits of the new downhole reservoir network solution include:

  • A permanent gauge installation providing life-of-well data and cost-effective, low risk access to diagnostics data from the reservoir section of a well. The result is a compelling alternative to traditional production logging, wireline, coil tubing and other cable-based downhole solutions that have accompanying risk, costs and logistics.
  • The ability to retrieve pressure and temperature data from multiple reservoir sands in a pilot hole – something that was previously not possible – leading to an improved understanding of reservoir connectivity and drainage.
  • Online zonal flow data measurements without having to reduce flow rates and without the limitations of intervention-based systems, with the added ability to wirelessly operate flow control valves in multiple locations in response to zonal data acquisition.
  • The fast and seamless installation of the interface to the network with no additional penetrators (wet mates, connectors, tubing for fiber, etc.) to go through the defined well barriers (thereby significantly reducing risk) and no additional hardware requirements to the topside or subsea control system. Instead, operators have a single standard interface card providing access to all the in-well instrumentation.

For more information, visit visit the Intelligent Multistage Completion Network page here.

Presse :
• Contacts : Contacts presse monde pour Emerson

Ressources supplémentaires :
• Rejoignez la Communauté Emerson Exchange 365
• Suivre Emerson sur X Facebook LinkedIn YouTube

À propos d’Emerson 
Située à Saint-Louis dans le Missouri (États-Unis), Emerson (NYSE : EMR) est une société internationale de technologie et de logiciels, qui propose des solutions innovantes aux industries essentielles du monde. Grâce à son portefeuille de produits d’automatisation de pointe, dont sa participation majoritaire dans AspenTech, Emerson aide les fabricants de produits hybrides, de procédés et discrets à optimiser leurs opérations, à protéger le personnel, à réduire les émissions et à atteindre leurs objectifs de développement durable. Pour en savoir plus, rendez-vous sur Emerson.com.

Activez JavaScript pour utiliser ce site Web.