Emerson delivers faster, easier configuration of HART® devices and streamlined wireless network management

AMSDeviceManagerv13

AMS Suite: Intelligent Device Manager version 13.0 helps users Build wireless network infrastructure easily while ensuring reliability and efficiency

Asset management software decreases start-up and turnaround times for HART devices and helps users build more reliable wireless networks

AUSTIN, TEXAS (May 13, 2015) – Emerson Process Management’s AMS Suite: IntelligentDevice Manager​ version 13.0 software enables customers to configure HART devices in bulk, saving time and reducing errors. Managing wireless networks is also easier as users can expand wireless networks faster and with more built-in reliability.

Users can now quickly and reliably standardize asset configuration for both HART and FOUNDATION™ fieldbus devices, simultaneously applying features, options, and alerts to an unlimited number of devices, in a fraction of the time. Built-in validation reports automatically compare configurations and quickly identify when devices deviate from the associated template. After commissioning, changes can be applied in bulk to modify or fine tune device configurations. With both HART and FOUNDATION​ fieldbus devices, bulk configuration reduces time to fully configured devices by up to 80% compared to existing work practices.

“Customers are under constant pressure to start up their plants more quickly to deliver product,” said Peter Zornio, chief strategic officer of Emerson Process Management. “Emerson is committed to delivering technology to promote engineering efficiency and help our customers reduce risk to project schedules and budgets.”

AMS Device Manager version 13.0 also features the AMS Wireless SNAP-ON™ application which allows users to identify liabilities in network setup and receive critical device and network health alerts. For organizations with an increasing wireless network footprint, network splitting is simplified. It is easy to identify where to put a new gateway, evaluate all existing devices on any number of networks, and receive guidance on organizing devices for maximum efficiency. Making structural changes is as simple as dragging and dropping devices between networks.

About Emerson Process Management

​Emerson Process Management (www.EmersonProcess.com), an Emerson business, is a leader in helping businesses automate their production, processing and distribution in the chemical, oil and gas, refining, pulp and paper, power, water and wastewater treatment, mining and metals, food and beverage, life sciences and other industries. The company combines superior products and technology with industry-specific engineering, consulting, project management and maintenance services. Its brands include PlantWeb™, Syncade™, DeltaV™, Fisher®, Bettis™, Micro Motion®, Rosemount®, Daniel™, Ovation™ and AMS Suite.

About Emerson

Emerson (NYSE: EMR), based in St. Louis, Missouri (USA), is a global leader in bringing technology and engineering together to provide innovative solutions for customers in industrial, commercial, and consumer markets around the world. The company is comprised of five business segments: Process Management, Industrial Automation, Network Power, Climate Technologies, and Commercial & Residential Solutions. Sales in fiscal 2014 were $24.5 billion. For more information, visit Emerson.com.

Activez JavaScript pour utiliser ce site Web.