Emerson to supply Westinghouse more than $8M in safety-related Fisher control valves for SCANA nuclear power plant in South Carolina

Valves in critical nuclear island applications and in the passive residual heat removal system will help ensure effective reactor operation and a high level of plant safety


MARSHALLTOWN, IOWA (August 18, 2011) – Westinghouse Electric Company has awarded Emerson Process Management more than $8 million in purchase orders for critical control valves to be used in two AP1000® pressurized water reactors at SCANA Corporation’s Virgil C. Summer Nuclear Generating Station in Jenkinsville, South Carolina. With site preparation already under way, construction is scheduled to begin late this year or early next year.  The two new reactors are scheduled to begin commercial operation in 2016 and 2019, respectively.

Emerson was selected for this project based on its experience in producing valves for the same applications in other AP1000 plants.  The Fisher® control valves covered by the purchase orders are identical to those selected for the first four AP1000 nuclear power units being built in China and two additional units in the US Southeast.

Fisher air-operated control valves will serve as part of the safety-related system in the nuclear containment area.  Engineered to comply with ASME Section III standards for components of nuclear facilities, they undergo rigorous qualification testing at the new Emerson Innovation Center in Marshalltown, Iowa.  Valve actuators are sized in accordance with EPRI (Electric Power Research Institute) guidelines to ensure adequate operating margins that meet industry standards. They are also designed and tested to survive vibration loads of six times gravity in three axes to confirm they can operate after a seismic event. 

For the passive residual heat removal system, Emerson developed a specially modified ball valve that meets all specified flow requirements and fits in the limited space available. These valves have received extensive testing to prove their ability to provide highly efficient flow through natural convection without assistance from the reactor coolant pump.  Testing has also demonstrated tight valve shut-off when the plant is in operation to maintain efficiency and accurate throttling control for all flowing conditions.

About Emerson’s Nuclear Valve Experience

For over 35 years, Emerson has supported nuclear facilities worldwide with Fisher nuclear valves and associated services. In fact, Fisher valves are installed in over 90% of the world’s nuclear facilities. To date, thousands of Fisher ASME Section III N-Stamped and RCCM process control valves have been installed around the globe.

About Emerson Process Management

Emerson Process Management (www.emersonprocess.com), an Emerson business, is a leader in helping businesses automate their production, processing and distribution in the chemical, oil and gas, refining, pulp and paper, power, water and wastewater treatment, mining and metals, food and beverage, life sciences and other industries. The company combines superior products and technology with industry-specific engineering, consulting, project management and maintenance services. Its brands include PlantWeb™, Syncade™, DeltaV™, Fisher®, Micro Motion®, Rosemount®, Daniel, Ovation™, and AMS Suite.

Mídia:
• Contatos: Contatos de mídia global da Emerson

Outros recursos:
• Participe da comunidade Emerson Exchange 365
• Siga a Emerson no X Facebook LinkedIn YouTube

Sobre a Emerson 
Emerson (NYSE: EMR) é uma empresa global de tecnologia e software que fornece soluções inovadoras para os clientes dos mercados industrial, comercial e de consumo. Por meio de seu portfólio de automação, que é líder de mercado, além de sua participação majoritária na AspenTech, a Emerson ajuda fabricantes híbridos, de processo e discretos na otimização de suas operações, na proteção de seus funcionários, na redução de emissões e na realização de metas de sustentabilidade. Para mais informações, acesse Emerson.com.


Ative o JavaScript para usar este site.