Emerson’s wellhead pressure monitoring technology will be used to enhance safety during the multi-year Tyra field redevelopment project. Photo courtesy of Total E&P Danmark.
High resolution image
Wellhead pressure monitoring used as safety measure during the installation of replacement platforms and topsides during two-year redevelopment
ESBJERG, DANMARK (Nov. 25, 2019) – Total E&P Danmark A/S has awarded Emerson a contract to provide wellhead pressure monitoring technology to enhance safety during the multi-year redevelopment project to extend the life of Danmark’s biggest gas field.
The Tyra field in the Danish part of the North Sea has been in production for more than 30 years but is today suffering from seabed subsidence. Since production started in the 1980’s, the seabed has subsided by more than five meters, reducing the air gap between the sea level and the bottom of the platforms. In order to keep the Tyra field in production, Total E&P Danmark is replacing the existing wellhead platforms with new and elevated topsides. The 13-meter-high jacket extensions and new topsides will be installed on top of the existing jacket structures.
The Tyra redevelopment project will ensure continuous production from Denmark’s biggest gas field, while safeguarding Danish North Sea infrastructure. The $3.3 billion investment in the redevelopment is the biggest ever in the Danish North Sea. Once completed, Tyra is expected to produce more than 200 million barrels of oil equivalent. The current Tyra field has two production complexes, Tyra East and Tyra West, which are linked to satellite fields Harald, Roar, Svend, Tyra Southeast and Valdemar.
During the two-year shut-in, Emerson technology will monitor wellhead casing pressures as a safety measure. With power and cable infrastructure unavailable, a wireless and battery-powered solution is required. Emerson will provide more than 200 Rosemount™ wireless pressure transmitters to be installed on the four riser platforms. The devices will transmit data to two standalone Emerson DeltaV™ PK Controllers, to be installed on the offshore accommodation platforms. Data will be presented to construction workers locally on human machine interfaces and relayed to an onshore monitoring point and data historian.
“Emerson’s wireless technology has been successfully deployed within offshore applications around the world, helping improve the safety of people and operations,” said Roel van Doren, president of Emerson Automation Solutions in Europe. “The ability to offer a complete solution capable of providing real-time measurement and awareness to help Total monitor and respond to pressure changes safely was a key factor in the use of Emerson technology.”
For more information about Emerson wireless solutions for wellhead applications, visit https://www.emerson.com/en-us/industries/automation/oil-gas/well-monitoring-integrity.