Emerson Launches Advanced Dust Pulse Technology Control System

The ASCO DPT Control System provides superior monitoring.

Included in the DPT Control System solution is the DPT P151 Controller, a modular control system designed specifically to provide efficient and reliable pulse-jet filter cleaning control.
High resolution image

The P152 DPT Particle Sensor is cost-effective for detecting leaks in dust collection systems.

The P152 DPT Particle Sensor is robust and cost-effective for detecting leaks in dust collection systems. High resolution image

The ASCO DPT Control System provides superior monitoring, optimizing dust collector system performance and increasing uptime

LAATZEN, Germany (Oct. 4, 2022)  – Emerson’s new ASCOTM DPT Control System optimizes the performance and improves the efficiency of filtration and dust collector systems by providing accurate and reliable low-level particulate monitoring, early warning leak detection, enhanced cleaning control and real-time diagnostics. The connected system serves as a cost-effective, scalable and purposeful step toward a facility’s digital transformation. It is now available in Asia-Pacific, Europe and Middle East and Africa regions, with availability in the Americas by mid-2023.

Using traditional sensing technology, low-level leakage is hard to detect in environments with high operating pressure, high humidity or oil and steam. The advanced signal processing of the DPT Control System helps ensure accurate, low-level measurement and detection of particles of less than 1 milligram per cubic meter in harsh, high-pressure (maximum 7 bar) and high-humidity applications, like those found in the cement, power plant, incineration, finishing aluminum and chemical industries.

“The digital transformation of the process industry is underway and connected facilities around the world are seeing the valuable sustainability and operation cost reducing benefits that real-time monitoring and diagnostics deliver,” said Stephan Cocciardi, director of marketing and global strategic accounts with Emerson’s discrete and industrial business. “The sophisticated monitoring capabilities of the ASCO DPT Control System can help facilities detect issues and prevent problems that would otherwise waste energy and accrue unplanned downtime, resulting in a more efficient and reliable dust collection system.”

By closely monitoring dust collector systems in real time, the DPT Control System can help users locate and address leaks before they become issues, improving energy efficiency and compressed air consumption savings. The loop-powered sensor enables intrinsically safe monitoring of difficult-to-access points of the filtration system, including coil, diaphragm and filter bag. The system’s condition monitoring and predictive maintenance capabilities can improve system reliability and efficiency while reducing maintenance costs and unplanned downtime. Its superior linear output can help users track real-time particle emissions levels and meet emissions regulations.

In addition to monitoring, the DPT Control System optimizes the performance and uptime of dust collector systems of all sizes through efficient and reliable pulse-jet filter cleaning control. For facilities that use large baghouses, application-specific control algorithms can reduce pulsing frequency, which can extend filter life and reduce the amount of compressed air consumed. The control logic can maintain quite low and stable differential pressure during operation and automatically maintains differential pressure within ±25 Pa (±0.1 inch) of water column of set point while minimizing pulsing. This ensures consistent cleaning performance, maintains a proper filter cake and can reduce compressed air use by 15% to 40% over standard, on-demand cleaning and up to 90% over continuous. It also helps ensure consistent airflow to maintain production, ventilation and dust recovery.

The system provides extensive general filter pulse jet cleaning control modes, such as easily selectable pulsing patterns and a full range of basic timing modes. Modes include continuous, high/low, single cycle and cycle down.

The complete DPT Control System solution includes the DPT P150 Particle Monitor, DPT P151 Controller and P152 DPT Particle Sensor. Learn more about the ASCO DPT Control System.

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via X Facebook LinkedIn YouTube

About Emerson 
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.

Voor gebruik van deze website moet JavaScript worden ingeschakeld.