New Tool Can Turn 50 Hours of Thermowell Design Time Into 15 Minutes

​Emerson's Rosemount thermowell design tool

Emerson's new Rosemount Thermowell Design Accelerator features a dynamically changing image that intuitively leads users through thermowell designs. High Resolution Image

Emerson’s Rosemount Thermowell Design Accelerator eliminates the largest pain point of temperature process design – manual thermowell iterations – significantly increasing operational efficiencies and cost savings

SHAKOPEE, Minn (May 11, 2020) – Emerson today introduced the Rosemount™ Thermowell Design Accelerator, a free online thermowell design tool that eliminates manual thermowell iterations facing process design engineers when sizing thermowells. It is easy to use and intuitively guides users through complex projects, saving hours of wasted labor and resources. Users will be able to automatically iterate up to 1,000 thermowell tags with a single click – all optimized for their process conditions.

On average, engineers can spend 50 hours doing thermowell calculations for a single project. Nearly 20 variables related to process conditions and thermowell dimensions are used to find a safe and efficient solution. Temperature points often need to be recalculated three to four times using traditional trial-and-error methods before passing global standards for safe operation outlined by The American Society of Mechanical Engineers (ASME). Using the Thermowell Design Accelerator, engineers can reduce design ideation time to just 15 minutes.

The software uses ASME PTC-19.3 TW (2016) criteria and has built-in quality checks to confirm safe thermowell results that protect processes and the people that operate them. As the tool automatically iterates thermowell dimensional changes for safe use, it also tracks calculation history. Engineers get a breakdown for each thermowell iteration and the corresponding physical dimensional change to the thermowell as it calculates solutions. Engineers can review each step for how the thermowell was able to pass PTC criteria and have a reference for updating their design if process conditions change. It’s true design, not just thermowell pass or fail.

Thermowell Design Accelerator is easy to use. The onscreen image dynamically updates as tag data is input and the onscreen help feature identifies potential calculation issues like missing data or incorrect inputs. Plus, users get thermowell and matching sensor specification model codes for a quick and easy way to review, collaborate, purchase and share information with project teams.

Thermowell Design Accelerator is part of Emerson’s portfolio of engineering tools, designed to help engineers quickly and confidently design solutions. It can be accessed anytime online at www.emerson.com/ThermowellDesignSoftware and designs can be saved in the MyEmerson personalized digital experience.

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via X Facebook LinkedIn YouTube

About Emerson 
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.

Voor gebruik van deze website moet JavaScript worden ingeschakeld.