LNG Users Maximize Space, Reduce Costs with New Pressure Relief Valves

​Relief valve, prv valve, pressure regulator, LNG, natural gas storage tank, Anderson Greenwood, pilot operated relief valve

Emerson's Anderson Greenwood 9300H low pressure pilot operated pressure relief valve.
High resolution image


End users can fulfill overpressure protection requirements with smaller valve

STAFFORD, TEXAS (September 25, 2018) – Emerson is helping LNG marine transportation customers to reduce their initial pressure relief valve investment at the shipyard by up to 25 percent, and total cost of ownership with its new Anderson Greenwood™ 9300H low pressure pilot operated pressure relief valves (POPRVs). The Anderson Greenwood 9300H patented design provides leak-free operation up to set pressure with an additional 10.5 percent flow capacity over valves currently available on the market. The additional capacity reduces the required size of the valve providing initial purchase savings, with additional savings on the associated piping, fittings and expansion elbows.

Designed specifically for marine LNG tanks on ships, floating production or storage units, the valve allows ship owners and operators to efficiently fulfill their critical overpressure protection requirements with smaller-sized valves and associated piping. The 9300H provides the superior performance and seat tightness of Anderson Greenwood POPRVs and utilizes the 52-year, field-proven Anderson Greenwood 93 Series pilot mounted flush to the valve providing a rugged, low profile ideal for rough seas. The valve is field-adjustable for either modulating action to reduce product loss during a relief event or snap action to open completely at set pressure. The 9300H valves can be easily equipped with valve monitoring technology and are certified for liquified gas carrier applications by all major classification societies, including Lloyd’s Register, American Bureau of Shipping, Bureau Veritas, and Det Norske Veritas.

According to Bloomberg New Energy Finance’s Global LNG Outlook, long-term global LNG demand is projected to “grow between 4-7 percent annually and a potential shortage can only be relieved by final investment decisions on new export projects in 2018-20.” 

“LNG continues to play an increasing role in global energy,” said Brett Bockeloh, product manager for pressure relief valves, Emerson Automation Solutions. “As the world pushes to keep pace with growing LNG demand, the need for innovative, reliable overpressure protection solutions has never been greater. The Anderson Greenwood 9300H’s combination of performance and reliability puts our customers in the best position to achieve their goals without the need to compromise on safety or their budget.”

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via X Facebook LinkedIn YouTube

About Emerson 
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.

​​​​​​​
Voor gebruik van deze website moet JavaScript worden ingeschakeld.