Water is used to cool the tuyeres that inject air into the blast furnace. The flow of cooling water at the inlet and outlet of the cooling circuits is monitored to determine if there is a leak in the cooling circuit, which would show up as a difference between the two flows. The flow measurement must be as accurate as possible to quickly identify a leak, and reliable to prevent unnecessary alarms and shutdowns.
A leak in the cooling water circuit changes the dynamics of the cooling system, impacting the reaction in the furnace, and decreasing the performance and efficiency of the furnace. If the leak is not detected in a timely manner and water is injected into the furnace, hydrogen is produced resulting in dangerous safety conditions and causing erosion in the furnace walls and roof that can be expensive and time consuming to repair.
The Rosemount™ 5408 Non-Contacting Radar Level Transmitter uses enhanced technology and Human Centered Design to deliver accurate, reliable measurements on both liquid and solid materials. Using two-wire FMCW technology the Rosemount 5408 deploys a continuous echo to maximize radar signal strength and produce a more robust and reliable measurement. Delivering ease-of-use at every touch point, the Rosemount 5408 uses an intuitive software interface to guide the operator through installation, commissioning, proof-testing and maintenance. Safety certified to IEC 61508 for SIL 2 applications, the Rosemount 5408:SIS reduces cost of risk, increases efficiency and protects people and the environment.