How It Works

Eliminate Hardware for FAT

The CSLS and the rest of DeltaV SIS with Electronic Marshalling hardware components can be virtualized to enable the configuration and testing of the entire DeltaV SIS system in a high-fidelity virtual environment.

Simulated SLS are easily configured on ProfessionalPLUS and Application Stations, and support both simplex and redundant configurations. Simulate for SIS also supports both local and global peer-to-peer communications of secure parameter references.

Ship Hardware to Site Earlier

Since hardware is no longer required for configuration development or software FAT, all hardware can be shipped directly to site. This not only reduces cost but eliminates project-schedule dependencies.

No Changes Needed for Transfer

Configuration does not require modification to be transferred to physical components.

Virtual CSLS uses exactly the same code as the physical CSLS, and the configuration does not require any modification to be transfer to the physical system.

Transferring SLS configuration between on-line and simulation environment is easy using export/import functions. 

By examining the module CRC, users can make sure safety logic was not impacted when transferring to the physical system.

The Latest

Edge Software Enhancement Helps Safeguard Data and Ensures Continuous Process Visibility

Emerson’s DeltaV™ Edge Environment has been updated to include a new “Store and Forward” feature, which minimizes risk and reduces costs by...

Emerson Enhances Control System Software for Seamless Data Integration, Improved Operational...

DeltaV distributed control system update features expanded connectivity via Ethernet-based protocols and streamlined state-based control execution

Scalable Technologies Pave the Path to the Next Great Lithium Battery Advancements

Emerson expert Kenny Marks , senior business development manager of the process systems and solutions business, shares his view on how...
Włącz skrypt JavaScript aby skorzystać z tej strony internetowej.