Wireless PeakVue Plus Refinery

CONDITION MONITORING CASE STUDY | PETROCHEMICAL

Petrochemical Company Anticipates Avoiding Millions of Dollars in Unplanned Repairs by Using Software Embedded with Expert Knowledge

       

PeakVue PLUS Technology for Machinery Analysis
PeakVue PLUS Technology for Machinery Analysis


For nearly three decades, Emerson’s PeakVue™ has been recognized as the premiere technology for detecting rolling element bearing. 

PeakVue Plus is a patented extension of PeakVue, going a step further to provide prescriptive analytics – allowing personnel with no special training in machinery diagnostics to easily act or suggest actions to avoid machinery failures. 

Explore PeakVue


 

RELATED CONTENT


Top 5 U.S. Power & Utility Company Reduces Labor Costs & Improves Reliability with Wireless Vibration Monitoring & Analysis Software
 

Emerson’s AMS Wireless Vibration Monitors, AMS Machine Works, PeakVue Technology and more helps propel Power & Utility customer into the future.



READ CASE STUDY




RELATED CONTENT


Chemical Manufacturer Avoids Dangerous Failures by Monitoring Vibration and Employing Analysis Software Tools


Emerson’s Machinery Health Software and AMS 6500 Machinery Health Monitor with embedded PeakVue Technology help refiner avoid downtime.



READ CASE STUDY




Business Results

  • Avoiding pump seals failure that could lead to $8M in unplanned labor and materials expenses
  • Estimated savings of $9.6M in installation and commissioning of 800 sensors
  • Safety improvements and labor savings via automated data collection

Application

Centrifugal Pumps used for metering in the refinery.

Customer

Petrochemical company, United States

Challenge

A refinery petrochemical complex with over 450 critical centrifugal pumps had been collecting pump vibration data manually every 90 days. To improve safe conditions and reduce pump-seal failures, the team sought improved condition monitoring techniques. Their goals included reducing pump-related Loss of Primary Containment (LOPC) events and meeting company reliability wins.

Solution 

The customer team recognized that by automating the collection of vibration data and enhancing vibration analysis, they could predict issues well in advance of failure and could address the needs before vibration caused damage to the pump seals.

Teams from the customer, Emerson, and Puffer Sweiven (Emerson’s local Impact Partner) collaborated to add an AMS Wireless Vibration Monitor, which delivers full vibration data over a self-organizing wireless mesh network. In addition, for a full complement of pump-related analysis and prescriptive analytics, the team included expertise-embedded software — PeakVue technology and the Plantweb™ Insight pump application.

PeakVue technology prescribes the necessary corrective actions to preserve bearing life and ensure long-term asset availability. The Plantweb Insight application displays real-time pump status and alerts using machine learning based asset models and analytics to provide early warning of pump cavitation, gear wear, and more. Alerts are sent to the team, who can address the condition of these critical pumps.

Prescriptive analytics specifically for pumps will enable insights that reduce Loss of Primary Containment (LOPC) events.

Project Manager, Rotating Machinery

The wireless, battery-operated transmitter gathers data at a defined time of day without manual intervention and enables the team to capture trends and be alerted to problems. If conditions require, an alert is immediately sent to the operator or to the system to shut down the pump.

To make the analysis even more robust, the collaborating teams added data gathered by pressure, temperature, and flow measurement devices to the vibration monitoring system. The Plantweb Insight software takes advantage of these digital transformation advances. Data is gathered, artificial intelligence driven by expert design analyzes the data, and alerts are automatically distributed to the right people at the right time.

The complete solution — including gathering data, storing data, analyzing data, and acting on information — is through a single source, Emerson, who has designed all elements to work together without fail. Collaboration by the teams ensured its success.

Get Started

Request a consultation to discover how Emerson's team of condition monitoring experts can help you initiate, expand, or improve your current program or projects.

Voor gebruik van deze website moet JavaScript worden ingeschakeld.