Media Resources
Emerson is helping our customers meet their operating, sustainability, and business performance goals. Find out how.
To meet increasing demand for greenhouse gas reduction and vital sustainability targets, companies are looking to adopt hydrogen as a flexible, renewable energy source. Emerson delivers environmentally sustainable solutions for customers across the hydrogen value chain, from production to transmission and storage, to distribution and consumption. The right technologies can help improve productivity, reduce variability, decrease energy usage, lower emissions and validate the sustainability of operations across the value chain.
PosHYdon is the world’s first offshore green hydrogen production project. This initiative integrates three energy systems on the world's first fully electrified platform in the Dutch North Sea.
Electricity generated by offshore wind turbines is used to power the hydrogen plant on the platform, converting seawater into demineralized water, and then into hydrogen via electrolysis. The 1 MW electrolyzer will produce a maximum of 400 kg of green hydrogen each day. The green hydrogen will then be mixed with gas and transported via existing gas pipelines to the coast, minimizing environmental impact.
Emerson’s DeltaV Supervisory Control & Safety System and instrumentation are in this case not only providing seamless integration of the three renewable energy data systems but also, ensuring safe operations in fluctuating offshore environments.
The pilot aims to gain experience in integrating working energy systems at sea and the production of hydrogen in an offshore environment. The insights gained will support efficient, large-scale offshore hydrogen production by 2030-2035, and consequently transforming energy production methods.
“Hydrogen is the future of a diversified and environmentally sustainable energy mix, but we need a balanced, accelerated approach across the entire value chain to make this ambitious goal a reality. This means building a solid foundation that combines automation technologies, collaboration with domain experts, and using existing infrastructure to help accelerate hydrogen’s development as a reliable energy source.”
Mike Train,
chief sustainability officer at Emerson
Frequently Asked Questions about Hydrogen
Hydrogen, or H2, is an element that makes up about three quarters of all matter in the universe. Although it is the most abundant substance in existence, hydrogen is rarely found on Earth in its pure form, so it must be extracted using other energy sources. Because hydrogen has three times as much energy content by weight as gasoline, it can enable net-zero or near net-zero emissions when produced from renewable sources or paired with carbon-capture technologies.
As a fuel, hydrogen is converted into energy by means of traditional combustion or electrochemical fuel cells or blended with natural gas for use in power generation applications, residential heating, or mass transportation in trucks, trains, ships and aircraft. Hydrogen is also used as a raw material in a wide range of industries, including oil refining, pharmaceuticals, metals manufacturing, and methanol and ammonia production.
Today, 99% of all hydrogen is produced from fossil fuels such as natural gas or coal via gasification or steam methane reforming with CO2 as a byproduct. Carbon capture, utilization and storage (CCUS) technology can then be applied to remove greenhouse gases, resulting in so-called blue hydrogen. Hydrogen can also be made from electrolysis, which applies an electrical current to water molecules, splitting them into oxygen and hydrogen with zero carbon emissions. Most electrolysis is powered by the existing electricity grid, but if renewable sources such as wind or solar are used, the resulting “green” hydrogen can provide the same.
Hydrogen is an extremely versatile fuel that offers a path to sustainable long-term economic growth. It can add value to multiple sectors in the global economy by serving as a sustainable fuel for transportation and manufacturing, and an input for the production of electricity and heat for homes. Industry experts project that a $2.5 trillion global market for hydrogen technologies could exist by 2050, with 3.4 million jobs added in the U.S. alone. Furthermore, renewable hydrogen could cut global CO2 emissions by 25% if produced at scale.
But to achieve full commercialization, key challenges related to cost, durability, reliability, performance, and lack of infrastructure must be addressed. New technologies, such as electrolyzers with greater output capacity, must be further developed and expanded into larger markets for hydrogen to compete with fossil fuels or wind, solar and nuclear energy in terms of life-cycle cost, performance, durability, learning rates and environmental impact. Non-technical barriers also need to be addressed, such as developing codes and standards, establishing best practices for safety, and developing a robust supply chain and workforce.
Get your Accelerating the Transition to Hydrogen Fuel e-book detailing the solutions to key challenges OEM's face in hydrogen processes. In this e-book, you will learn about:
Complete the form to access your complimentary copy of our Accelerating the Transition to Hydrogen Fuel e-book today.