Operators in industries that produce significant amounts of dust during the manufacturing process are faced with the challenges of achieving precise level measurements during production and preventing overfills. Dust buildup can not only interfere with the accuracy of some devices, but also contributes to the buildup of heat inside small spaces, like hoppers. Vibrations created by running machinery can also compound the problem. Operators need reliable, robust level measurement solutions that are made to handle the extreme conditions found in dusty environments.